AXIS#.BODE.INJECTPOINT
Description
AXIS#.BODE.INJECTPOINT sets whether the excitation uses current or velocity excitation type.
AXUS#.BODE.INJECTPOINT | Description |
---|---|
0 | None |
1 | Current |
2 | Velocity |
Example
Code
Set AXIS1.BODE.INJECTPOINT to current:
--> AXIS1.BODE.INJECTPOINT 1
Get AXIS1.BODE.INJECTPOINT (already set to current):
--> AXIS1.BODE.INJECTPOINT 1
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 2 |
Default Value |
0 |
Data Type |
Integer |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.BODE.INJECTPOINT | 0x5001 | 0x1 | USINT | - | - | RW | False |
AXIS2.BODE.INJECTPOINT | 0x5101 | 0x1 | USINT | - | - | RW | False |